Skip to main content

Policumbent

 

Policumbent is a student Team from Politecnico di Torino, born in 2009, which aims to beat the world speed record for human-powered vehicles. The team is made up of bachelor’s and master’s degree engineering and design students. It is divided into several areas that work together to design and build the most efficient vehicles on Earth.

 

Our mission is to design and build prototypes to beat the world speed record for human-powered vehicles. In doing so, the entire team studies and works together to reduce at their minimum the mechanical and aerodynamic dissipations. In the last three years, its members are also using this knowledge for a completely new urban-mobility project, which will have a fully bio-based aerodynamic fairing made of flax fibers and 100% bio-based resin, making it fully recyclable and natural.

In its history, the team has won several editions of the World Human Powered Speed Challenge (WHPSC). It set the second highest speed in the female leg-powered vehicle and man trike arm-powered vehicle categories, both being also Italian speed records, respectively with 123.88km/h and 82.88km/h. It also holds the Italian record for the man leg-powered vehicle reaching 136.49km/h.

For more information about our project please visit this website; https://www.policumbent.it/en/